Motor_L_detected
| Index.Sub | 2005.9H |
| Data Type | Unsigned32 |
| Access | Read/Write |
| PDO Mappable | No |
| Unit | H x10-6 |
|
Range |
Unsigned32 |
| Default Value | -- |
| Store Supported | No |
| Description |
This object returns the motor L (inductance) detected with Motor R,L detection function (bit#9 of Drive_Working_Settings_Extended object equal to 1). The Nominal_Current of the motor must be defined. |
|
Notes |
|